PKR39809-02

Inrush Restraint Operation

Inrush Restraint works by raising the Phase, Earth and NPS threshold current settings for a short period of time to allow the inrush current to subside.

NOTE: Inrush Restraint does not affect SEF thresholds or settings configured for Definite Time tripping.

Apart from the On/Off control there are two settings that determine how Inrush Restraint operates as shown in the below:

Setting

Default

Description

Inrush Restraint Time

0.10 s

The time Inrush Restraint will remain active once triggered.

Inrush Restraint Multiplier

X4

Setting current multiplier while Inrush Restraint is active.

  • Inrush Restraint is armed for operation whenever the load current goes to zero.

  • When the load current goes from zero to non-zero, the Inrush Restraint is activated and the Inrush Restraint Multiplier is applied to the Phase, Earth, and NPS pickup thresholds for the Inrush Restraint Time.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.