PKR39809-02

UOF Protection

UOF protection is an optional protection element that can be configured to trip the switchgear if the measured frequency deviates above or below acceptable levels for user-set times.

UOF protection can also be configured to automatically reclose the switchgear after an UOF protection trip if the system frequency has returned to within a normal frequency band.

UOF elements have separate On/Off controls so that either or both can be operational at any one time.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.