PKR39809-02

System Settings 2

System Settings 2

Options Available

Options Not Available

P

   

Once the device has been initially configured, the menu can be de cluttered by making Options unavailable which removes the ten Options pages.

The Switchgear Status page contains mainly read only fields relating to the condition of the device.

The Work Tag can also be applied from this screen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.