PKR39809-02

Appendix K.6 ­ setVUE ACR and AS Automation Menu Screens

This appendix shows all of the Automation display group pages and lists display options and setting ranges.

The Automation display group can consist of between 3 and 8 pages depending on the configuration when Loop Automation is available or 3 pages when Auto-Changeover is available.

The Automation display group does not appear in the menu structure by default. It is only displayed when either of the two automation features, Loop Automation and Auto-Changeover has been made available. These features are mutually exclusive.

Table 145 setVUE Automation Menu Pages for ACR and AS

Automation Menu

Loop Automation

Auto-Changeover

Loop Automation Status(1)

Auto-Changeover Configuration(2)

Loop Automation Configuration 1(1)

Auto-Changeover Communications(2)

Loop Automation Configuration 2(1)

Auto-Changeover Communications Stats(2)

Loop Automation Configuration 3(3)

 

Loop Automation Configuration 4(4)

 

Loop Automation Configuration 5(5)

 

LA Communications(6)

 

LA Downstream Communications(7)

 

LA Tie Communications(8)

 

(1) Only displayed when Loop Automation is available.

(2) Only displayed when Auto-Changeover is available.

(3) Only displayed when Loop Automation is available and Device Type is Tie.

(4) Only displayed when Loop Automation is available, Logic is Intelligent and Tie Control is Message.

(5) Only displayed when Loop Automation is available, Device Type is Tie and Logic is Classic.

(6) Only displayed when Loop Automation is available and Logic is Intelligent.

(7) Only displayed when Loop Automation is available, Logic is intelligent and Device Type is not Tie.

(8) Only displayed when Loop Automation is available, Logic is intelligent and Device Type is Tie.

The top line of each page is the page title. To the right of the title is the letter A which indicates that the page being displayed is part of the Automation display group.

The next three lines are the data or information on display. Most displays have six data fields. The standard layout is shown below.

When Loop Automation is available, the first page to be displayed in the Automation menu is the Loop Automation Status page.

When Auto-Changeover is available, the first page to be displayed in the Automation menu is the Auto-Changeover Configuration page.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.