PKR39809-02

LAN 1 and LAN2 (Ethernet)

The PowerLogic ADVC Controller has two 100Base-T Ethernet ports each with a baud rate of 100 M bits per second. Their physical ports are RJ45 female connectors.

The Ethernet ports can be used to run WSOS or supported communications protocols over TCP/IP.

The PowerLogic ADVC Controller implements an on-board switch to provide the support for 2 LAN interfaces.

NOTICE
HAZARD OF LOSS OF COMMUNICATION OR UNRESPONSIVE CONTROLLER
If both the LAN ports are configured, it is essential that they be configured with IP addresses for 2 distinct subnets.
Failure to follow these instructions can result in equipment damage.
NOTICE
HAZARD OF LOSS OF COMMUNICATION
If the controller is connected to a LAN or Wide Area Network (WAN) then it is strongly recommended that:
  • Fire walls be used to limit user access to the controller
  • Ethernet switches be used to limit the volume of Ethernet data reaching the controller’s 100Base-T port (Use of Ethernet hubs is not recommended).
Failure to follow these instructions can result in equipment damage.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.