PKR39809-02

Disabling APGS

Certain operator actions will cause APGS to be disabled.

  • A change to the Power Direction setting.

  • Selection of an active protection group other than Protection Auto.

  • Setting APGS to Not Available.

Table 41 APGS Settings/Specifications

Automatic Protection Group Selection Settings/Specifications

Auto Change Time

10...180 s

Auto Change Time Resolution

1.0 s

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.