PKR39809-02

Event Log on the flexVUE

The flexVUE O.I. has a dedicated EVENT LOG key. Pressing this key is the only way the Event Log can be displayed on the flexVUE O.I.

When the Event Log is initially displayed the Event Log header appears on the top line and only one event, the most recent, is displayed on the bottom line.

Note that on the initial Event Log page shown above, the time stamp has a resolution of 1 minute and the event is truncated.

To view the complete Date/Time stamp with a resolution of 10 ms, press the Left Arrow key.

Pressing the Right Arrow key from the initial display will enable the complete event description to be viewed. See below:

If the complete event description is longer than the 20 characters available, the display will automatically scroll to reveal the entire event.

Once scrolling is commenced by pressing the Up Arrow key, separate events can be viewed on each line. If the log is scrolled via the Down Arrow key until the end or most recent event is displayed the Event Log header will reappear on the top line. In this way the most recent event can be identified.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.