PKR39809-02

Measured Values

The PowerLogic ADVC Controller measures up to 10 power system components:

  • A, B, and C phase current.

    • From CTs in each phase of 3 phase switchgear.

  • Sensitive earth/ground current (three phase switchgear only)

    • A measurement of the spill current in the common connection between the three CT secondary currents on the PCOM board.

    • Only used for SEF protection/detection up to 80 A primary and not displayed as an analogue measurement.

  • Phase to Earth voltage on all six terminals (if available)

    • From CVT built into all six bushings on RL Series and PMSet UR Series switchgears. Or from the I bushings on PMSet U Series switchgears.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.