PKR39809-02

Time Zone

The Time Zone feature allows the PowerLogic ADVC Controller to be configured for the time zone where it is located. It also allows the system time to be automatically adjusted for daylight saving during certain times of the year.

Time Zone is an optional feature that must be made available through feature selection before it can be used.

In WSOS: Display > Configuration > Feature Selection > General

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.