PKR39809-02

SEF Directional Protection

When SEF Directional Protection is enabled, it can use one of three methods to determine the direction of a SEF.

  • VZPS

  • Wattmetric

  • Ir Cos (Ø)

VZPS is the default option. The Decision setting determines the method used. Operating Quantities, Fault Angles and default Characteristic Angles for each method are shown in the table below.

Table 52 Directional Protection SEF Polarising Methods

Polarising Method (Decision)

Operating Quantity

Fault Angle

Angle logged on Trip

Default Characteristic Angle

VZPS

Earth Current (Ir)

VZPS → IZPS

VZPS → IZPS

VZPS → IZPS

Wattmetric

Residual Power

VZPS x IZPS x Cos (FA)

VZPS → IZPS

VZPS → IZPS

VZPS → IZPS

Ir Cos (Ø)

Active Earth Current

IZPS x Cos (FA)

VZPS → IZPS

VZPS → IZPS

VZPS → IZPS

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.