PKR39809-02

PowerLogic ADVC Controllers General Arrangement

PowerLogic ADVC Controller withflexVUE O.I..

Figure 354
PowerLogic ADVC General Arrangements

The setVUE and flexVUE Operator Interfaces are available with PowerLogic ADVC.

NOTE: If the Fast Trip Input Module (FTIM) is required it must be specified at the time the device is ordered.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.