PKR39809-02

Configuration

Once this feature has been enabled, the operator will be able to configure the actions required for each protection element, either OFF, Alarm or Trip.

These options are available for the following Protection elements:

  • Phase Overcurrent

  • EF

  • SEF

  • NPS

The additional settings are displayed on the WSOS Control page shown in the Figure 126.

Figure 126
WSOS Per Element Protection

Per Element Protection can also be configured on the operator interface.

The table below explains the changes that occur with the protection elements affected when Per Element Protection is enabled. It assumes that Protection is ON, Sensitive EF Protection is available, Sequence Components are available and NPS OFF is allowed.

Table 27 Per Element Protection Available/Not Available

Element

Per Element Protection Not Available

Per Element Protection Available

Phase

Phase protection is always On (when Protection is ON).

Phase protection can be ON (Trip), Off or Alarm.

Earth

EF protection can be ON (Trip) or OFF.

EF protection can be ON (Trip), OFF or Alarm.

SEF

SEF protection can be ON (Trip) or OFF.

SEF protection can be ON (Trip), OFF or Alarm.

SEF Alarm

SEF Alarm can be ON or OFF.

SEF Alarm can be ON or OFF. (no change)

NPS

NPS protection can be ON (Trip), OFF or Alarm.

NPS protection can be ON (Trip), OFF or Alarm. (no change)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.