PKR39809-02

Overview

The CLT provides the user with an opportunity to develop additional logic functionality for the PowerLogic ADVC Controller Range. By evaluating user-defined collections of digital and analogue data points from the existing protocol database, the CLT is used to alert operators of specific conditions that may exist on-site. Based on these conditions, it is also possible to program basic actions automatically if required.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.