PKR39809-02

Conditional Auto Reclose Configuration

Conditional Auto Reclose must be made available before it can be used.

In WSOS this feature can be made available by selecting:

Display > Configuration > Feature Selection > Protection > Conditional Auto Reclose Available.

On it can be made available on the operator interface.

Once Conditional Auto Reclose has been made available it can be configured with a single setting: Conditional Auto Reclose Timeout.

This setting determines the maximum time that can elapse between when the ACR trips and when a conditional automatic reclose can occur.

To configure this setting in WSOS go to:

Display > Protection > Universal Settings.

The Conditional Auto Reclose Timeout setting can also be configured on the operator interface.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.