PKR39809-02

Navigation

The Panel On key turns the O.I on or off. An optional door switch is available to turn the O.I on when an operator opens the door and off when the door is closed. If the controller is fitted with this option the button can be used to turn the O.I off/on while the door is open. Closing the door will turn the O.I off.

Lamp Test tests all LEDs on the O.I. The purpose of this is to alert the user to any LEDs or colors that may not be working correctly.

Event Log displays the event log on the LCD display.

The Menu key enters the menu structure from where an operator or engineer can display data and modify settings.

The arrow keys are used to navigate through the structure and to change settings. The UP and DOWN arrows scroll through the available options, RIGHT to progress to the next level and LEFT to return to the previous level. The Select key is used to select fields to be changed and apply values when changes are made.

For more information on how to navigate around the flexVUE menu see Appendix J flexVUE menu.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.