PKR39809-02

Automatic Reclose

An automatic reclose is effectively a check to see if a fault that caused a protection trip is still on the line. The ACR can check one, two, or three times before giving up depending on how the auto reclose settings have been configured.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.