PKR39809-02

Cold Load Status on Power Up

The CLP status can be changed from the status display by changing the time.

Consider a situation where the load has been off and the controller powered down for some hours due to module replacement/maintenance etc.

The controller was powered down during the outage so when it is powered up again it assumes the load to be diverse that is the Operational Cold Load Time is zero and the CLP status will be Idle.

Because the CLP status time is an operator setting it can be manually adjusted to reflect the duration of the outage and thus allow for the load that might occur when the ACR goes back into service.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.