PKR39809-02

Event Log

The PowerLogic ADVC Controller maintains a log of up to 30,000 events that reflect changes to the status of the switchgear, control electronics, and programmable logic. The log also records setting changes.

The events can be viewed on the LCD display. The event log display will update automatically with new events. The most recent event appears on the bottom line of the screen and older events can be viewed by scrolling upwards. When the event log is full, the newest events replace oldest events.

All events are date and time stamped to a 10 ms resolution and displayed in the order that they occurred. The source of each event is also recorded.

It is possible to apply event category filters when viewing events. WSOS software can also be used to upload and display the event log. WSOS also supports source identification and filtering as well as text and Date/Time searches. The uploaded event log can be saved as a text or .csv file.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.