PKR39809-02

First Screen Selection

When standard menus only are used, the first screen seen by an operator on power up is selectable from any page in the menu.

Selection of the first screen can only be made through WSOS

Display > Configuration > Menu Configuration

If the custom menu is used, and rotating screens mode is active, the first screen feature is overridden.

If the custom menu is used, and the first screen selected is unavailable in the menu then the controller will default to the Trip Flags screen.

If the standard menu is active, the selected screen might still not be available if the feature associated with that screen has been made Not Available or Not Allowed in Feature Selection.

In this case the Trip Flags will be the first screen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.