PKR39809-02

GFN Configuration

If required to be used, GFN must firstly be made available through feature selection.

This can only be done in WSOS at:

Display > Configuration > Feature Selection > Protection > GFN Available.

Once GFN has been made available it can be enabled and configured in WSOS by opening the Protection page and selecting Universal Settings.

Figure 156
WSOS GFN settings

GFN is configured with the following settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.