PKR39809-02

Event Sources

The source of an event can vary. For example, a Work Tag Applied/OFF setting change event could have been triggered from IOEX, the O.I., local WSOS5, remote WSOS5 over TCP/IP, or SCADA protocol.

If the ALT key is pressed whilst the event log is on the display then the date and time details are replaced with extra information that includes the source. Pressing the Alt key again will red is play the date and time information.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.