PKR39809-02

CLP Summary

  • The user-set Cold Load time and Cold Load Multiplier are protection settings, only the Cold Load Status/Time is an operator setting.

  • Only the protection elements that are selected, Phase, Earth, SEF, and NPS, are affected by the Cold Load Multiplier.

  • Definite Time settings are not affected.

  • CLP cannot be used if normal load currents are expected to drop below 2.5 A.

NOTE: It is possible for Cold Load and Inrush Restraint to be applying multipliers at the same time.

In this situation, Inrush will use the Operational Cold Load Multiplier if it is the higher.

Table 45 CLP Settings/Specifications

CLP Settings/Specifications

Cold Load Multiplier Range

1...5

Cold Load Multiplier Resolution

0.1

Cold Load Time Constant Range

1...480 minutes

Cold Load Time Constant Resolution

1 minute

Timing Accuracy

± 1 minute

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.