PKR39809-02

User Guide

When the CLT configuration tool opens, a new menu entitled CLT logic tool will appear in the WSOS main menu bar.

From this menu, the user guide for the CLT can be downloaded by selecting Open Manual.

NOTE: Faster CLT The CLT functionality used to have an inherent 500 ms delay in evaluating expressions that used on any of the controller’s Analogue data as a data point. With version A50-11.xx, we have now introduced a new class for Analogue data points, under Appendix A_10. These appear as 40 ms Analogs in the Logic Expression Builder tool and are available for use within the CLT only.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.