PKR39809-02

Earth VZPS Polarizing

With VZPS polarization, the operating quantity is earth current (3 x IZPS) and the fault angle is the zero sequence current angle with respect to the zero sequence voltage angle (VZPS → IZPS).

For demonstration purposes, the figure below substitute’s residual current and voltage for zero sequence current and voltage. Although they have different magnitudes, the angles are the same.

Figure 165
EF Current and Voltage Phasors

This figure shows phasor diagrams for voltage and current during a hypothetical purely resistive A phase to EF on an earthed neutral system.

The fault causes A phase voltage to reduce and the residual voltage phasor is 180° out of phase as shown.

The current in A phase is increased and the residual current phasor is in phase with A phase current.

The fault angle for this fault is 180° that is the residual current is 180° out of phase with the residual voltage.

The actual fault angle for an EF is determined by the network characteristics (line resistance and reactance, neutral earthing arrangement) and the fault characteristic (such as the nature of the short-circuit – solid or arcing, fault impedance and earth resistance).

Earth VZPS Characteristic Fault Angle

The default Characteristic Angle for Earth Directional Protection is +135° . So an A phase to EF where the residual current led the residual voltage by 135° would be a forward fault in the centre of the forward sector.

The Characteristic Angle setting for Earth VZPS polarising is configurable between -179° and 180°.

A typical Characteristic Angle for systems with solidly or impedance earthed transformer neutrals would be approximately +135°.

If this fault occurs when Protection Groups A and B are active the Event Log would record:

  • Forward Pickup Earth

  • Protection Group A Active

  • Forward Earth Protection Trip

  • Angle at Fault 135°

  • Polarising Voltage at trip VZPS

  • Polarising Voltage at the maximum VZPS

The same fault in the opposite direction would record:

  • Reverse Pickup Earth

  • Protection Group B Active

  • Reverse Earth Protection Trip

  • Angle at Fault -45°

  • Polarising Voltage at trip VZPS

  • Polarising Voltage at the maximum VZPS

Earth VZPS Sector Width

The default Forward and Reverse Sector Width settings for earth protection are both 90°. These are ± settings and equate to actual sector widths of 180°.

Sector Width settings are identical for all elements and Decision settings. For more information, refer to Sector Width.

Earth VZPS Low Polarising Voltage Action

In order to determine the direction of an EF that caused a pickup when VZPS polarization is used, the controller expects Zero Sequence Voltage to be above the Earth Low Threshold setting.

The Low Threshold is one of two settings that deal with low polarising voltages. The other is the Low Polarising Voltage Action.

If the polarising voltage is below the Low Threshold setting for EFs, the Low Polarising Voltage Action setting will determine what action must be taken.

The options are:

  • Use Forward

  • Use Reverse

  • No Action (default setting)

More information on the No Action option can be found here.

The Earth Low Threshold setting can be configured for between 15...15,000 Volts.

When Use Forward or Use Reverse actions are selected, a fault with low polarising voltage will cause a trip as though it was a normal fault in the selected direction. The only indication that the polarising voltage was low would be the Polarising Voltage at trip VZPS event which would record a value lower than the Earth Low Threshold setting.

When No Action is selected, an EF with low polarising voltage will cause a pickup followed by a Polarising Voltage Low VZPS event reporting the low value of polarising voltage. It will not cause a protection trip. The pickup condition will remain active until the fault resets.

Earth VZPS Low Voltage Reset

Once the polarising voltage has been deemed to be Low, it will not return to Normal until either the fault resets or the measured polarising voltage exceeds the Low Threshold setting by 10%. So if the Low Threshold setting is 500 VZPS and a Low Voltage condition exists, VZPS will have to rise to 550 VZPS before the Low V condition is cancelled.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.