PKR39809-02

Per Element Protection + Extended Standard Protection

When Extended Standard Protection is also made available, the operator can configure the per element action on a per group basis as shown in the figure below. The configuration can be unique to each Protection group and will become effective when that group is made active.

The features of the Extended Standard Protection still apply. Refer to Extended Standard Protection for details on this feature.

Figure 128
Extended Protection settings

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.