PKR39809-02

QAKs

QAKs are configured by left clicking with the mouse on the QAKs to be configured.

Selecting the QAKs for Live Load Blocking (d1) will open the dialogue box below:

Figure 52
Customize QAKs

This dialogue can be used to:

  • Change the name (Label Description) of the QAK.

  • Change the Lamp Function Logic that determines the True and False states.

  • Change the Key Action Logic that determines the action caused by pressing the key.

  • Set the colors to represent True and False states.

  • Determine if the status must be displayed when the O.I. is off.

  • Determine if the key must be still active when the O.I. is off.

  • Determine if the key action is controlled by the Unlock Key status.

There are two Logic Expression Builders associated with configuring a QAK and they are opened by selecting the fx buttons for each logic field.

The Logic Expression Builder for the lamp function is the same as for the Status Lamps.

There is a different Logic Expression Builder for the Key Action Logic.

Figure 53
Logic Expression Builder for QAKs and Lamp

All data points available to be assigned to this QAK can be found by expanding the tree structure in the Data Points field. The following features are also provided:

  • A Find box is provided to make finding specific points easier.

  • Expressions can be built using the Point Values provided to determine if pressing the key must turn the selected function on, turn it off, or toggle through the available options.

  • A formatting button is provided to delete all text if required.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.