PKR39809-02

Weekly Maximum Demand

The controller maintains a log of Weekly Maximum Demand records that show the total energy for the week as well as the peak power and the period during which it occurred. The most recent record i.e. the previous week, is displayed by default. The Date/Time displayed is the end of the period when the peak average power was logged.

Weekly Maximum Demand

Total energy for the week (kWh)

The date at the end of the week

 

Date/Time for period of peak power

 
   

Peak power and power factor

 

Earlier records can be viewed by pressing the SELECT key to enter the history mode and navigating using the Left and Right Arrow keys.

When earlier records are being displayed, the title changes to:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.