PKR39809-02

Negative Phase Sequence (NPS) 4

4NPS protection can only be used if Sequence Components are available.

The NPS elements are driven by the NPS current (I2) which is calculated in real time by digitally summing the phase currents sampled every 5 ms and applying the Fortescue formula for sequence components.

An NPS pickup occurs when the measured current ≥ the NPS setting current x the NPS pickup multiplier. A tripping time is calculated based on the magnitude of the fault current and the settings for the active trip. While the pickup is active, tripping times are calculated for each sample. Unless the fault resets, a protection trip will ensue.

NPS pickup, reset thresholds and multiplier settings are global that is they apply to all trips. Timing is determined by settings configured individually for Trips 1...4, Single Shot and Work Tag.

Table 37 NPS Protection Configuration Options

NPS Configuration Settings

Range/Options

Resolution

Default

Global Settings

Setting Current

10 A...1260 A

1.0 A

40 A

Pickup Multiplier

1.0...10.0

0.1

1.0

Reset Threshold Multiplier

90%...100%

10%...100%(1)

1.0%

90%

Per Trip Timing Settings

Curve Options

Inverse Time Curves

3 x IEC255 Refer Appendix D

3 x IEEE Refer Appendix E

42 x TCC Refer Appendix F

Up to 5 User Defined Curves

IEC255 Standard Inverse

Other Curves

Definite Time Instantaneous Only

Inverse Time Curve Modifiers

Time Multiplier

0.01...25.00

.01

1.00

Instantaneous Multiplier

Off, 1.0...30.0

0.1

Off

Minimum Time

0.00...2.00 s

0.01 s

0.00 s

Additional Time

0.00...30.00 s

0.01 s

0.00 s

Maximum Time(2)

Off, 0.2...180.0 s

0.1 s

Off

Other Curves

Definite Time

0.01...100.00 s

0.01 s

1.00 s

Definite Time Instantaneous Multiplier

Off, 1.0...30.0 s

0.1 s

Off

Instantaneous Only

x 1.0...x 30.0

0.1

1.0

Instantaneous Minimum Time

0.00...2.00 s

0.01 s

0.00 s

(1) Reset Threshold Multiplier setting range is 10%...100% when Reset Curves are available.
(2) This is a global setting unless Extended Minimum Time per Curve is on.
 

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.