PKR39809-02

IOEX Configuration

There are two database points available in the IOEX Configuration Toolbox that can be used to build an IOEX map for use with Conditional Auto Reclose.

Digital Controls (IOEX Input)

Name

Description

Conditional Auto Reclose

This point is checked prior to each Auto Reclose only when the Conditional Auto Reclose feature is available.

If this point is high, then an automatic reclose is allowed. Otherwise the reclose is delayed until this point goes high providing it does so within a configurable time out period. If the time out period expires before this point goes high the ACR will go to lockout.

Digital Data (IOEX Output)

Name

Description

Trip Request

This point is set when a Trip Request is issued.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.