PKR39809-02

NPS Alarm Configuration

In WSOS this setting can be configured on the Control page.

The NPS Alarm can also be selected on the operator interface. Auto Reclose On/Off.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.