PKR39809-02

Options

In its standard configuration the PSM will always provide one AC auxiliary supply input. At the time of order it is possible to specify an auxiliary supply voltage of
115 Vac or 230 Vac. The voltage is pre-set in the factory. The voltage is indicated on the controller rating plate. If necessary, it is possible to swap the voltage setting in the field from 230 to 115 or vice versa. If this is done the rating plate will need to up updated to show the new rating.

The standard PSM includes a single 115/230 Vac auxiliary supply input with circuit breaker, toroidal transformer, filter, and terminals. A battery circuit breaker is always fitted as well.

The PSM cover design includes space for the different circuit breaker combinations that can result from the supply options mentioned above. Removable panels are located in the cover. To make sure these panels are not accidentally pushed out, the panels are held in place with small tabs that have to be snapped off, using pliers, before they can be removed.

IEC power outlet – An IEC power outlet can also be fitted in the chassis.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.