PKR39809-02

WSOS Only Features

Some WSOS features are WSOS only and not supported by the controller.

  • Launch pad

  • Switchgear explorer

  • Switchgear navigator

  • Switchgear status

  • Automatic data retrieval (ADR)

    NOTE: Enhancement to ADR can be configured in WSOS to retrieve data from multiple controllers on a regular basis. Prior to version 5.16.25, data retrieval over a TCP/IP connection was done in a sequential manner, where in WSOS would connect to each controller one at a time to retrieve the data configured via ADR. With 5.16.25, this task has been modified to allow WSOS to establish simultaneous TCP/IP connections to multiple controllers. GEX69813.
  • Operator Log

  • Communications Output Log

  • Display and printing of settings

  • PowerLogic ADVC Controller firmware loader

  • Communication statistics

  • Settings retrieval and storage

  • Settings export/import

  • Configurable Protocol Tool

  • IOEX Editor

  • Intelligent Loop Automation Schemes

  • NTP Setup

  • SCADA Communications Diagnostics

  • Batch Change Configuration

  • OCP Configuration Tool

  • CLT

  • DNP3 Secure Authentication

  • Four user password levels - operation, telecontrol, protection, and system

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.