PKR39809-02

Status Lamps

The Status Lamps are used to indicate the controller and switchgear status. All 20 lamps are configurable and users can choose to change the default configuration. WSOS includes a tool to modify the logic function for each lamp and a utility to print new labels. Please see flexVUE customisation for more information.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.