PKR39809-02

Display

The flexVUE O.I. features a two line x 20 character display. The menu that runs on this interface organizes the individual pages into display groups.

It is possible to navigate to any page and to view or change settings using the navigation keys located to the right of the display.

Figure 14
flexVUE O.I. Navigation keys and Display

The top line of the display shows the title of the menu or sub-menu and is always in capital letters.

The bottom line may display a sub-menu of the menu on top line in which case it will also be in capitals.

When the bottom line is not in all capitols it indicates that it is a read-only or editable field.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.