PKR39809-02

Attempt Count

This is a read-only field which displays the number of attempts that have been made to connect to the master station.

An attempt will call each of the PSTN numbers in the list until a connection is established. An attempt ends after either the DCD line is asserted, or all numbers in the Telephone Numbers list have been dialled.

NOTE: The Attempt Count does not indicate the number of phone calls made.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.