PKR39809-02

Sync Check Configuration

Once the Sync Check feature has been enabled, its settings are configured independently for each protection/detection group. However, the Voltage, Frequency and Phase ON settings are read-only and cannot be configured independently. Additionally, the Sync Check settings in the forward group are copied to the reverse group when Directional Protection/Detection is enabled.

DANGER
HAZARD OF UNSYNCHRONIZED NETWORK
Perform Sync Check when there are several sources in the network and they need to be interconnect with each other.
Failure to follow these instructions will result in death or serious injury.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.