PKR39809-02

Appendix K.4 ­ setVUE ACR Protection Menu Pages

This appendix lists all of the Protection display group pages.

The basic Protection display group consists of 26 default pages.

Up to 96 additional pages can be added to the protection menu depending on the features that have been enabled.

The table below shows the complete list of available pages and their position in the protection menu.

Table 143 setVUE Protection Menu Pages

Protection Menu

Default Pages

Additional Pages

Alternate Pages

Protection Setting 1...3

   

Protection Setting 4(1)

   

Protection Setting 5, 6

   
 

Protection Setting Alarms 1, 2

 
 

Protection Setting 7(2)(3)

 

Protection Setting 8(8)

   
 

Protection Setting 9(5)

 

Cold Load Pickup Protection

 
 

Sync Check Settings 1 - 4(6)

 
 

Directional Blocking Phase 1, 2(7)

Directional Protection 1(8)

 

Directional Blocking Earth(7)

Dir Protection Phase 2, 3(8)

 

Directional Blocking SEF(7)

Dir Protection Earth 4, 5(8)

 

Vzps Compensation(7)

Dir Protection SEF 6, 7(8)

 

High Vzps Alarm(7)

Vzps Compensation(8)

   

High Vzps Alarm(8)

 

Phase Threshold Trip No 1(9)

 

Phase Protection Trip No 1

   
 

Phase Protection Reset No 1(10)

 
 

Phase Threshold Trip No 2(9)

 

Phase Protection Trip No 2

   
 

Phase Protection Reset No 2(10)

 
 

Phase Threshold Trip No 3(9)

 

Phase Protection Trip No 3

   
 

Phase Protection Reset No 3(11)

 
 

Phase Threshold Trip No 4(12)

 

Phase Protection Trip No 4

   
 

Phase Protection Reset No 4(11)

 
 

Phase Single Shot Threshold Trip(12)

 

Phase Single Shot Prot Trip

   
 

Phase Single Shot Prot Reset(11)

 
 

Phase Work Tag Threshold Trip(12)

 

Phase Work Tag Prot Trip

 
 

Phase Work Tag Prot Reset(11)

 
 

Phase Protection Max Times(13)

 
 

Earth Threshold Trip No 1(12)

 

Earth Protection Trip No 1

   
 

Earth Protection Reset No 1(11)

 
 

Earth Threshold Trip No 2(12)

 

Earth Protection Trip No 2

 
 

Earth Protection Reset No 2(11)

 
 

Earth Threshold Trip No 3(12)

 

Earth Protection Trip No 3

 
 

Earth Protection Reset No 3(11)

 
 

Earth Threshold Trip No 4(12)

 

Earth Protection Trip No 4

 
 

Earth Protection Reset No 4(11)

 
 

Earth S Shot Threshold Trip(12)

 

Earth Single Shot Prot Trip

 
 

Earth Single Shot Reset(11)

 
 

Earth W Shot Threshold Trip(12)

 

Earth Work Tag Prot Trip

   
 

Earth Work Tag Reset(11)

 
 

Earth Protection Max Times(13)

 
 

SEF Threshold Trip No 1(12)

 

SEF Protection Trip No 1

   
 

SEF Protection Reset No 1(11)

 
 

SEF Threshold Trip No 2(12)

 

SEF Protection Trip No 2

   
 

SEF Protection Reset No 2(14)

 
 

SEF Threshold Trip No 3(11)

 

SEF Protection Trip No 3

   
 

SEF Protection Reset No 3(15)

 
 

SEF Threshold Trip No 4(16)

 

SEF Protection Trip No 4

   
 

SEF Protection Reset No 4(15)

 
 

SEF Single Shot Threshold Trip(16)

 

SEF Single Shot Protection Trip

   
 

SEF Single Shot Prot Reset(15)

 
 

SEF Work Tag Threshold Trip(16)

 

SEF Work Tag Protection Trip

   
 

SEF Work Tag Prot Reset(15)

 
 

SEF Protection Max Times

 
 

NPS Threshold Trip No 1(16)

 
 

NPS Protection Trip No 1(17)

 
 

NPS Protection Reset No 1(18)

 
 

NPS Threshold Trip No 2(17)

 
 

NPS Protection Trip No 2(18)

 
 

NPS Protection Reset No 2(19)

 
 

NPS Threshold Trip No 3(17)

 
 

NPS Protection Trip No 3(18)

 
 

NPS Protection Reset No 3(19)

 
 

NPS Threshold Trip No 4(17)

 
 

NPS Protection Trip No 4(18)

 
 

NPS Protection Reset No 4(19)

 
 

NPS Single Shot Threshold Trip(17)

 
 

NPS Single Shot Protection Trip(18)

 
 

NPS Single Shot Prot Reset(19)

 
 

NPS Work Tag Threshold Trip(17)

 
 

NPS Work Tag Protection Trip(18)

 
 

NPS Work Tag Prot Reset(19)

 
 

NPS Protection Max Times(19)

 
     
 

Under/Over Frequency Protection 1,2(20)

 
 

Rate of Change of Frequency(20)

 
 

NVD Protection 1, 2(20)

 
 

NVD Alarm 1, 2(21)

 
 

Broken Conductor Protection(21)

 
 

Broken Conductor Alarm(21)

 
 

Under Voltage Protection(22)

 
 

Over Voltage Protection(22)

 
 

Under/Over Voltage Protection(22)

 
 

Under/Over Voltage Protection(22)

 
 

Fault Locator(23)

 
 

Conductor Characteristics(24)

 

(1) Not displayed when Per Trip Thresholds are available.

(2) Only displayed when Extended Standard Protection On.

(3) Not displayed when Per Element Protection is available.

(4) Only displayed when either Close on Fault Trip or Per Element Protection are available.

(5) Only displayed when Ground Fault Neutralizer is available.

(6) Only displayed when Sync Check available.

(7) Only displayed when Directional Blocking is available.

(8) Only displayed when Directional Protection is available Directional Blocking and Directional Protection are mutually exclusive.

(9) Only displayed when Per Trip Thresholds are available.

(10) Only displayed when Reset Curves are available.

(11) Only displayed when Reset Curves are available.

(12) Only displayed when Per Trip Thresholds are available.

(13) Only displayed when Extended Maximum Time per Curve is on.

(14) Only displayed when Reset Curves are on.

(15) Only displayed when Per Trip Thresholds are available.

(16) Only displayed when Per Trip Thresholds and Sequence Components are both available.

(17) Only displayed when Sequence Components are available.

(18) Only displayed when Sequence Components and Reset Curves are available.

(19) Only displayed when Sequence Components and Extended Maximum Time per Curve are on.

(20) Only displayed when Under/Over Frequency Protection is available.

(21) Only displayed when Neutral Voltage Displacement is available.

(22) Only displayed when Broken Conductor is available.

(23) Only displayed when Under/Over Voltage Protection is available.

(24) Only displayed when Fault Locator is available.

The top line of each page is the page title. To the right of the title is the letter P which indicates that the page being displayed is part of the Protection display group.

The next three lines are the data or information on display. Most displays have six data fields. The standard layout is shown below.

If the standard menu is running, the protection menu can be accessed by pressing the Panel On key and then pressing the Menu key three times.

The first page to be displayed in the Protection menu is the Protection Settings 1 as shown below.

Protection Settings 1

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.