PKR39809-02

Sequence Reset Clears Fault Flags

There is an option to clear the fault flags on a sequence reset.

If fault flags are set during a sequence that doesn’t lead to a sectionaliser trip, those flags will clear when the sequence resets.

This helps to ensure that after a sectionaliser trip, only the flags that were set during the sequence that lead to the trip are displayed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.