PKR39809-02

Status Indication

Synchronization indicators on the Measurement page in WSOS provide a quick visual check of the current synchronization status of the load and source voltages.

Status is displayed using four indicators for Global, Voltage, Frequency, and Phase.

When the indicators for all three components are green the source and load side supplies are synchronized. In this case the Global indicator will also be Green.

A component is synchronized when it is within the configured limits.

Figure 231
Synchronization Status displayed by WSOS

One or more components out of sync will cause the Global indication to appear out of sync as well as shown in the figure below.

Figure 232
Out of Sync indications displayed by WSOS

Synchronization status indicators can also be viewed on the flexVUE O.I. at:

Engineer Menu > Measurement Menu > Synchronisation.

Figure 233
Synchronization Status Indications on the flexVUE O.I.

Synchronization status indications appear on the setVUE O.I. in the Measurement menu.

Figure 234
Synchronization Status Indications on the setVUE O.I.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.