PKR39809-02

LOP Protection Configuration

LOP protection can be configured in WSOS on the LOP page:

Display > Protection > LOP

Figure 172
WSOS LOP settings

LOP protection can also be configured on the O.I.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.