PKR39809-02

Changing Protection Settings on flexVUE

Once the first Active Protection Group setting is changed, the following screen will appear:

This message will be displayed if all the following are true:

  • Settings are changed within the ACTIVE PROTECTION GROUP.

  • The current setting is the first one to be changed.

  • Before changing this setting, all the current settings were ACTIVE in service.

Once this message appears there are three options:

  1. NO ACTION: The new setting will automatically go into service if the operator ignores the above message, turns the O.I. off or the interface turns off automatically.

  2. Press SELECT: If the operator presses the SELECT key, the new setting is put into service. The operator can continue to browse the menu. With all the current settings in active service, continuing to change settings will cause the operator to be prompted again when the first of the new settings is saved.

  3. Press the ARROWS: This will allow the operator to continue to browse and change settings with a view to eventually putting them into service as a group.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.