PKR39809-02

Bypassing the Delayed Operation

If the switchgear must be operated without any unnecessary delay:

  • Press the TRIP or CLOSE key a second time (with the countdown timer running).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.