PKR39809-02

System Settings 2 (AS)

System Settings 2

Options Available

Options Not Available

P

   

Once the device has been initially configured, the menu can be decluttered by making Options unavailable which removes the nine Options pages.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.