PKR39809-02

UOF Protection Summary

  • UOF can be configured to trip the switchgear if the measured frequency goes outside of a designated normal band for an unacceptable period of time.

  • UOF protection elements can be enabled/disabled individually.

  • Settings can be configured within the range 45 Hz to 65 Hz but individual settings must be chosen with respect to other settings and the dead-bands.

  • The ACR will not auto reclose after a UOF protection trip but can be configured to close automatically when the frequency returns to normal.

Table 61 Under/Over Frequency Protection Settings/Specifications

UOF Protection Settings/Specifications

Frequency setting range(1)

45...65 Hz

Frequency setting resolution

0.1 Hz

Accuracy (for sinusoidal input)

± 0.05 Hz

Frequency dead-band (hysteresis)

0.2 Hz

Number of under or over frequency cycles before tripping

2...1000

Frequency calculation

Once per cycle averaged over 2 cycles

Low Voltage Inhibit range

4...23 kV

Low Voltage Inhibit setting resolution

1 V

Normal Frequency Close Time

1...1000 s

(1) Under/Over tripping frequencies and normal frequencies are interlocked by software so that only viable settings are possible.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.